Question: |
Answer: The discharge resistance of the Panel Elements which are made of solid plastic are within the antistatic range, from 109 to around 1011 ohms. This means: when friction (rubbing) is applied, there is no build-up of static charge since the charged particles are effectively dissipated at the surface. In other words, electronic components placed on the surface will not be damaged. However, if charged particles are transferred from one component that is already statically charged to a second component that is lying on the surface, the ability of the panel to dissipate this additional charge is not sufficient to prevent damage from the additional charge. For this purpose, conducting or conductive materials would have to be used as the surface. |
Question: |
Answer: |
Question: |
The critical moment is when the water jet exits from the solid plastic worktops. Also, at the beginning of the cutting process, there is considerable chance that the surface will be damaged and, as a result, the starting point of the cut should not be in the immediate vicinity of the edge, but some way away from it.
|
If you have further technical queries about our products please do not hesitate to contact your local distributor or simply send a mail to info@item24.com