Question: 
Can standard stainless steel tubes be used in conjunction with item Bearing Sets 8 50 (conveyor systems)?

Answer:
Tests have shown that this is a realistic option with 50x3 tube made of 1.4301, inner diameter 44.8 mm.
These tubes are standard products and can be obtained from usual suppliers. The internal weld seam should be filed away before the bearing flange is inserted and the rough edges caused by sawing should also be deburred inside and out.
The advantage of steel tubes is that they are insensitive to damage from rough-edged materials to be transported and, as a result, maintain their attractive appearance even after long periods of use.

Question:
How is the gear ratio for the manual Lifting Column 200x170?

Answer:
The lifting spindle in the manual column has a  trapezoid thread with left-handed thread.
The direction of rotation is reversed by the bevel gearbox (ratio i = 1:1), i.e. clockwise rotation of the crank causes the movable part of the column to rise.
One revolution of the crank is equivalent to an upward movement of circa 3 mm.

If you have further technical queries about our products please do not hesitate to contact your local distributor or simply send a mail to info@item24.com